This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with THD+N in PCM4202

Other Parts Discussed in Thread: PCM4202

I am using the ADC PCM4202 and I have a problem with the THD+N:

THD +N rise up at high level of input signal. See the next figure (Blue: THD+N; Red: Input level):

 

I can’t get the -105 dB of THD+N that specifies datasheet.

My board has every decoupling capacitors like demo board although my input analog circuit is different from the demo board. See next figure:

 

 

 

The ADC is setting in slave mode, HPFD disable, dual rate with clock auto-detection and fSCKI = 256 fs, fs= 96 Khz.

 

How could I improve the THD+N in this conditions? Thanks very much.