Hello.
I need to use 6 slave (using CC8531) and as I know this IC can have maximum 4 slave.
So I would like to know, is it possible to use two master (cc8531) that have same audio source (from codec TLV320AI)?
I already tried to connect BCLK, WCLK, DOUT, SCL, SDA, and RESET pin from TLV320AIC3101 (codec) to 2 master (CC8531). But it seems that audio came out from each slave have ripple noise.
It seems like i2s data is corrupted. so can i2s communication in parallel mode?