The manual for the TLV320AIC32 states that after the power supplys are good, the RESET must be driven low for at least 10ns. Taken literary, that would mean that the RESET has a falling edge, then a rising edge after good power is reached.
I have a TLV320AIC32 that behaves exactly with this requirement. Other devices have RESET asserted LOW during the power supplys rising ( from standard POR device ), then the RESET is simply de-asserted 200ms after good power. In this case, the devices do not see any falling edge on the RESET line after good power. All other devices requiring a hardware reset are happy with output from the POR device.
This standard POR does not work on this one device, but it will work if a RESET is driven low, then high after good power.
Does anyone know the exact requirement of the hardware RESET.
Les