So last Friday I had this unit working with my Atmel SamG53. I2C still works, and whatever settings I program in still appear in the device, and on are echoed back to the software with the EVM-K.
Today, I have no word clock, and no bitclock despite the fact that I have not changed anything in my settings, software, and am using the exact same USB cables which must be working because the kit responds to the Software, and my I2C is working from the Atmel.
Most of the jumper settings are those taken from the app note http://www.ti.com/lit/an/spma042b/spma042b.pdf
Settings:
Reg Enable : 3.3 + 1.8 EN
USB Config Ext, USB Rst, Usb SPI, USB Mck, USB I2S, SW2: A0, A1, A2 "off" (Marked ON on the dip-switch package by the way...)
J6 - N; J14 - N; J15 - N;
JP3, JP4 (pull-ups) : Populated
JP5 : FSX
MCKLI : 2-3
JP8 : N
SW1 : SE; SW2 : CAP; VDD Sel Sel; IOVDD 1-2, W15+W16 Populated
IOVDD SEL ; 3.3V
J7 : 2-3
========
- It is not the initiation sequence.
- It is not lack of an ample input master clock (scope verified)
- All of the power LEDs are on, all of the test points read the correct voltages
- Word clock and bit clock are both floating at high