At which Register I can route the ADC Input to the digital effects?
In the block diagramm I see SW-D1 and SW-D3.
But I didn't find the register to route the signal in this way !
Up to now I choose the digital output of the TLV320 and connect it to the digital Input by hardware.
But for product i can't do in this way, becausein this case I need additional MUX and I haven't the space for it.
(The Application is very cost and space sensitive).
Much thanks for your help .....
Richard