Hello.
Regarding PCM1795 DAC, I want to know the Low ESR typed capacitors can be used as the decoupling capacitor for Vref. (VcomL, VcomR).
If not, please let me know why it is impossible to be used.
FYI, we found strange symptoms like followings
■ symptom - The voltage level of Vref at VcomL and VcomR is exceed 2.5V when supply voltage level (Vcc) is 5V. (about 3~4.5V)
■ condition - Vcc 5V, internal bias decoupling capacitor : ELNA 100uF 6.3V (PVO, LOW ESR)
There is no guidance on the datasheet.
Regards.