I am using the PCM1863 to capture audio signals, and getting some very strange results when I set the gain levels in the positive range at 6dB and above.
The graph below shows some of my findings. The input in all cases is an identical 300Hz signal. The shift in phase only has to do with my capture method, and is not an issue. The change in amplitude is the issue.
The blue line shows the signal at 0dB. This signal looks great. However, the orange signal, which sets the gain to +6dB shows an increase in amplitude in the positive side, and some kind of clipping on the negative side. The amplitude on the positive side is not quite the 2x you would expect, and the negative side is obviously clipped.
Increasing the gain to +7dB generates the grey line. The resulting amplitude on the positive side is closer to 0dB, and on the negative side is very clipped.
Pushing the gain to +8dB results in the yellow line, which shows almost no amplitude. Zooming in on the graph, there is an amplitude change, but it is obviously small.
I am capturing this data immediately after it comes off the ADC, with no processing.
I assume the PCM1863 is not intended to work this way. I have tried this in both differential and single-ended mode with similar results.
Is there a setting I'm missing somewhere? How come the gain doesn't work as expected?
Thanks,