Just to verify, the TLV320AIC3106 has individual attenuation on each audio / analog input channel as shown in Figure 31. This says each channel has "a gain programmable from 0 dB to –12 dB in 1.5 dB steps". It also says, "In general, the mixed signal should not exceed 2Vpp (single-ended) or 4Vpp (differential)".
I'm just using one differential channel per PGA/ADC (Line2L_in, for instance. I don't plan on using channels 1L or 3L.
Is it fair to assume that before attenuation the signal cannot exceed 4Vpp (differential)? I'm assuming this is the case, but it would be great if the signal coming in could be 12 dB higher and it is attenuated -12 dB to the range 4Vpp (differential). This would increase the input voltage to: 4Vpp(diff) * 10^(12/20) = 4Vpp(diff) * 3.98 = 15.9V(diff) in.
Depending on the design of the attenuator, this could be the case or not & I can't find it specifically called out.
thanks,
David