AIC3106 connects to OMAP-L138 via I2S on TMDSEVML138 board. The stereo line outputs show noise.
AIC3106 registers are set in the following order:
0x00=0x00
0x01=0x80
0x02=0x22
0x03=0x40
0x07=0x0A
0x08=0xE0
0x09=0x40
0x0C=0x00
0x0F=0x00
0x10=0x00
0x13=0x04
0x16=0x04
0x1B=0x00
0x1E=0x00
0x25=0xE0
0x26=0x10
0x2B=0x00
0x2C=0x00
0x3A=0x00
0x48=0x00
0x52=0x80
0x5C=0x80
0x56=0x09
0x5D=0x09
0x65=0x01
0x29=0x50
Data input into DIN change in the following order:
A. all zero
B. 1kHz sin or cos
C. all zero
The traces of each A, B and C as follows:
A. all zero
B. 1kHz sin or cos
C. all zero
Which of the register configuration or the board design is the cause of the noise caused by? If caused by the register configuration, how should it be fixed?
Best regards,
Daisuke