Hi,
I would like to setup a aic3262 codec in multichannel mode. The serial-port ASI1 is driven by an external clock running at 2MHz with a 8kHz frame-sync. I would like the ADC to run at a sample-rate of 32kHz. The ADC will then have to send four stereo-pairs pairs per frame-sync to transmit all the 32kHz samples over the ASI1 interface. In the implementation I have setup the ADC for 32kHz sample-rate and the register B0_P4_R4_D[7:6] = 11 to get four stereo-pairs, but only one stereo-pair is transmitted over the serial port. Is it any additional settings needed to get all four stereo-pairs from the ADC?
Regards
/Björn Qvarnström