Hi,
I'm currently designing something around the AIC3254. The input would be fully differential from a dynamic mic (i.e. an SM58 or similar). I'm worried about noise with the PGA's turned up. A few questions.
1)Is there a less costly (but still programmable) alternative to using the PGA2505? I'm looking at the Maxim DS4420
2) If I were to use the PGA2505 as a preamp stage, how would I generate a dual supply (i.e. +15v -15v), given the low voltages involved (i.e. 1.8v/3.3vish from battery)
3) Can something be rigged up (albeit retaining low noise) with an opamp and a digital variable resistor to achieve a similar outcome?
Finally, if I wanted to also use phantom powered condenser mic's with the same circuit, how would I go about generating phantom power?
Thanks