Hi All,
I was redirected from the C67x Single Core DSP Forum with this question:
I am using the LCDKC6748 dev. kit with a TLV320AIC3106 codec on it. Unfortunately the codec uses capacitive coupling on LINEx/MIC inputs but I need dc coupling. This seems not possible with this codec because the LINEx inputs of the codec have DC bias voltage (around +1.3V). I removed and short cut the input caps but the CODEC measured -32768 only. Questions:
- Can the TLV320AIC3106 codec work with DC coupled single ended inputs? (non-capacitive coupling)
- If not then is there any TI CODEC (24-bit, 96kHz) which can be used for dc coupled inputs? I just need the simultaneously started 2xADC and 2xDAC. No DSP, no filtering. A codec which can be used for instrumentation application.
- It is shocking but I could not find the reference voltage of the ADC and DAC (TLV320AIC3106) in any manual. I also could not find the resolution of the ADC and the DAC in any manual. I think the resolution is 24-bit. Can somebody tell me in which manual specifies the resolution and the VREF?
Many thanks for your help!
Best regards,
Louis