Hi,
I am using a PCM4204 A2D converter. The datasheet front page specifies a maximum PCM sampling rate of 216 kHz and DSD rate of 64 Fs and 128 Fs. I am trying to determine the fastest data rate I can achieve with the device in DSD mode. Table 1 indicates that DSD is only available in Single or Dual rate, not in Quad rate - where I want to operate.
Is it possible to use the DSD at its highest rate to capture signals up to 100 kHz, or does the Single/Dual rate filtering prevent me from operating in this frequency band? What sampling mode and SCKI would result in the highest frequency DSD mode?
Thanks,
Jason