Hi forum!
I'm using a custom board with TLV320AIC3106 and igepv2 platform (DM3730 SoC). My system is linux 2.6.37
Basically I'm connecting this signals together:
- MCLK (in) to crystal 12.0MHz
- WCLK (out) to omap McBSP3_FSX
- BCLK (out) to omap McBSP3_CLKX
- DIN (in) to omap McBSP3_DX
- DOUT (out) to omap McBSP3_DR
The system is playing flawlessly and mixer seems it is working perfectly. When I try to capture (with a arecord command) I can only see wave header data without audio/raw data. Debugging BCLK and WCLK it's showing that there are no clocks.
Hope someone can help me, some clue on how to debug or go further it would be great.
Regards,
Sergio