Hi
Do you have a reference circuit of S/PDIF input?
There is just USB input reference circuit on the datasheet page26, to my regret.
Could you give me an S/PDIF interface circuit for PCM2903C?
Best Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
If you want optical S/PDIF (TOSLINK) that you can directly connect optical receiver like TORX147 from TOSHIBA or similar receiver from SHARP.
If you want isolated electrical S/PDIF that you need to use pulse transformer for isolation and some BUS receiver for converting of voltage level from S/PDIF to 3.3V CMOS level output. For consumer S/PDIF you will need termination resistor 75R and for professional S/PDIF 110R resistor. Pulse transformer suitable for S/PDIF is DA102C, LL1572, S22083 or PE-65612. For bus receiver I used 75176B but it has +5V TTL output. You need to find something with +3.3V level output. You can inspire on my page with soundcard based on PCM2902C. http://www.pavouk.org/hw/usbcodecpcm2902/en_index.html
When the chip detects correct S/PDIF signal that it automatically change input from ANALOG to S/PDIF.
Best regards, Pavel.
Pavel-san,
Thank you very much for your detailed explanation.
I understood well !!
Best Regards,
Pavel-san,
Sorry let me understand well about "isolation S/PDIF".
I think we usually use "Optical" or "Coaxial" interface.
In case of optical, we use Optical devices and in case of Coaxial, we use termination(75ohm or 110ohm)+Capacitor.
I do not know where we use "isolation" S/PDIF.
Could you tell me more detail?
Best Regards,
Hi Takumi,
If you use coaxial S/PDIF without isolation transformer that you can have troubles with ground loops between devices. It may cause bigger jitter of S/PDIF signal and hum or noise on analog part of your device. It is much better to avoid these possible troubles with using of pulse transformer on the S/PDIF inputs or outputs. Also combination with capacitor is good to prevent possible DC voltage on the input. For isolation are usually used these pulse transformers from more vendors: DA102C or LL1572 or S22083 or PE-65612. I tested them succesfully up to sample frequency 192kHz.
Best regards, Pavel.