Hi all
Would you mind if we ask TLV320DAC3101.
Our customer will only use the function speaker out of I2S input TLV320DAC3101.
And then, about VOL, our customer will only use Soft-VOL.
<Question1>
Without AVDD and HPVDD, is it possible to use the function speaker out?
We couldn't find the block diagram which related to AVDD and HPVDD.
So, is all of power(including AVDD and HPVDD) required to connect, isn't it?
<Question2>
In case of no use of followings pins, how does it should treat?
11 pin:VOL/MICDET- floating?
13pin:AIN1 - connection to GND?
14pin:AIN2 - connection to GND?
Kind regards,
Hirotaka Matsumoto