Hello
I'm new to this, and quite embarrassed to ask such elementary questions.
First, the manual sbau174 says in section 1.4 that the control software "comes with several script examples. . ." I cannot find these script examples in the codec control download. All I see for scripts is the initialization procedure. I'm sure I'm just not observing something obvious. Could you help me find these script examples?
Second, I am simply trying the "Play Back Digital Audio Signals via USB" test outlined in TI's SBAA179 Application Report on my PCM9211EVM-U boards. I am configuring the CodecControl path per Figure 7 of the application note. I attach a screen shot of my configuration
Here are my register settings as a result
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
00 00 01 04 00 01 81 00 03 0C FF FF 00 00 00 04
02 1A 22 22 00 02 0C 00 00 80 00 00 00 00 FF FF
C0 FF 00 00 00 00 D7 D7 00 00 FF FF FF FF FF FF
FF FF FF FF FF FF FF FF FF FF 00 00 00 00 00 00
44 10 00 00 00 00 00 00 00 00 00 44 00 00 0F 40
00 00 00 00 00 00 00 00 3D 00 00 00 00 00 01 FF
I have not changed any of the jumpers from the as-received condition.
My procedure is to simply try to read an output result for MPO0, while inputting a tone (4KhZ) from the pc through the usb. The tone is being provided by onlinetonegenerator.com through my PC. I clearly hear the tone when the usb is unplugged, and I carefully checked my sound settings on the control panel functions of my WIndows 7 PC so that USB is being output when the USB is connected.. My optical output is being analyzed with a Rohde&Schwarz Audio Analyzer DC . . . 110kHz. I detect nothing for my output. I did put an oscilloscope probe on the usb #3 pin, and note that the waveform changes a lot as the online tone generator is turned off and on. Once again, I'm sure I'm missing something very obvious.
I hate asking you these easy things, but can you help me to get my boards to output tones over S/PDIF coax or optical (coax preferred) ? Thanks in advance