Hi all,
Would you mind if we ask TLV320DAC3101?
<Q1>
Is there the starting sequence(restriction) of each power(AVDD, HPVDD, DVDD, IOVDD, SPLVDD) or not?
For Example) 1: AVDD 2: HPVDD, , , , , , , 5: SPLVDD
The data sheet P47 shows followings;
Define starting point:
(a) Power up applicable external power supplies
(b) Set register page to 0
We'd like to know about the sequence of "(a)".
<Q2>
How much of the time is it required between the starting sequence(restriction) of each power and the release of RESET?
(After all of the power turning on, until the reset will be released, is it required some wait time?)
<Q3>
How much of the time is it required between the release of RESET and the start of I2C control?
(After the release of RESET, from when is it able to start I2C control? Is it required some wait time after the release of RESET?
1ms?(like as the datasheet shows Device Start-Up Lockout Times)
Kind regards,
Hirotaka Matsumoto