Hi,
I can't success to run Windows AIC3105EVM GUI.
I have tested GUI on 3 PC: 2 running Win7 32 bits, and 1 with WinXP SP3. I think that drivers are installed correctly since no error message found in windows / hardware setting (USB-MODEMV / NI found).
Jumpers are set correctly, regarding settings found in EVM datasheet.
When I launch the GUI, I first get a windows that ask which AIC I am using, I select AIC3105, then the GUI window opens and immediatly close. I have tried win Win7 to set WinXP SP2 and XP3 compatibility, but I still get the same result: GUI opens and then immediatly closes.
Is there any option to make the GUI work ?
Thanks.