Hello D. Hartl, J Arbona, David Zaucha, Don Dapkus, Justin Bohr , and all engineers.
I have designed a PPS diagram in which an audio signal will flow to an enabled Biquad_1 filter before an output.
After I download the PPS diagram ( Bandpass filter is enabled) to AIC3254, I could hear the audio. Next, I want to change the Biquad_1 filter coefficient on the fly. So I wrote an SPI Arduino code to write to AIC3254. The Arduino code of disabling the Biquad_1 filter was the modification of the first box of an Appendix B in SLAA404C .
As a result, I just heard a loud noise.
Appendix B was also mentioned about adaptive filter, buffers and to enable DAC. I got confused on how to implement it.
Wasn’t AIC3254's DAC already power-up due to downloaded PPS diagram?
Please guide me on how is the proper way to change the biquad filter coefficient base on my setup? In before, I am successfully control the volume component of PPS using SPI Arduino without configuring processing block.
Thanks.
Kal