Hello,
I have some question of DIX4192.
When I use portB as a slave, is it necessary to synchronize it with MCLK?
If PortB aren't synchronizing with MCLK, does data will be dropped?
Input: Port B
Output: SPDIF(Tx)
Best Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have some question of DIX4192.
When I use portB as a slave, is it necessary to synchronize it with MCLK?
If PortB aren't synchronizing with MCLK, does data will be dropped?
Input: Port B
Output: SPDIF(Tx)
Best Regards,
Hi Justin,
Thank you for reply.
Datasheet say
"In Slave mode, the ports do not require a master clock because the left/right word and
bit clocks are inputs, sourced from an external audio device serving as the serial bus timing master."
There is mention mentioned above.
I thought that MCLK was not necessary.
However, it was necessary to input MCLK from a external audio device and understood when it was necessary to synchronize BCK and LRCK and MCLK.
Best Regards,
Kei