The feature list on the PCM1803A pages states:
Single-Ended Voltage Input: 3 Vp-p
The data sheet for the PCM1803A states:
Analog input voltage, full-scale (–0 dB) 3 Vp-p
It also states:
The differential voltage between VREF2 and AGND sets the analog input full-scale range.
There is no mention in the data sheet of what the VREF2 voltage should be. If I measure the VREF2 pin it is 5V. This implies the full scale voltage is 5V?
However, I am seeing with a signal of about 1.5Vpp the ADC is already outputting a full scale digital signal. If I exceed this voltage the waveform starts to clip.
The data sheet for the PCM1803 eval board http://www.ti.com/lit/ug/sleu061/sleu061.pdf (which may not be the same as the PCM1803A, but in general they are very similar) implies the maximum input is only 1Vrms (approximately 1.41Vp-p). It states, "Analog input up to 1Vrms is connected to CN103 and CN104." This would agree with what I have found experimentally.
So what is the full scale voltage?
Is it actually supposed to be 3Vp-p?
If yes, what are some reasons the signal seems to clip for me at about half that level?
I am operating the ADC in I2S slave mode if that makes any difference. Sample rate doesn't seem to make any difference.
Thanks,
Kevin