A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
AIC3204 current consumption in sleep mode : typo in datasheet
Hi,
I think their are some typ in the AIC3204 datasheet (dated November 2012).
I Quote :
"
2.9.1.1.1 Standby Mode (3.3V operation)
To put the device in standby mode, the AVDD and DVDD LDOs as well as the Reference Block (Page 1,
Register 123, D(2:0) = 101) must stay on, and all other blocks powered down. This state results in a
standby current of approximately 180mA. In standby mode, the device responds quickly to playback
requests.
2.9.1.1.2 Sleep Mode (3.3V operation)
In this mode all settings and memory content of the device are retained. To put the device into sleep
mode, the DVDD LDO must remain powered up (LDO_select pin), the AVDD LDO must be powered down
(Page 1, Register 2, D(0) = 0), the crude AVDD generation must be turned on (Page 1, Register 1, D(3) =
0) and the analog blocks must be powered down (Page 1, Register 2, D(3) = 1). The sleep-mode power
consumption is approximately 50mA
"
Is current consumption really in mA ??? Is it rather uA or nA ?
Thanks Nicolas