I'm in an rather unusual measurement situation, where both audio signals of a 10kHz bandwidth and a rather slowly changing voltage value are of importance:
Would a DC signal supplied to the audio input channels (of course not using the input capacitors) be sensed, and digitized correctly via USB?
If so, would simply biasing it around 0.5* Vccc, with a peak-to-peak voltage of 0.6 * Vccc suffice?
Also, I haven't been able to find crosstalk attenuation over frequency; am I just missing something?
Best regards,
Marcus Müller