Dear All,
i'm having a strange behavior on my PCM9211. All it's working fine, but the problem is the following:
if i choose my optical (RXIN2) or coaxial digital (RXIN0) and i play some music or i put them in pausa all works fine (this mean that i have a LRCK of 44.1KHz, BCK of 2.8MHz and a SCK of 11.3MHz). If i remove the connector the PCM9211 gives me a LRCK of 2.56KHz, BCK of 163KHz and a SCK of 655KHz).
All the relationship between the clock are ok (Fs, 64*Fs and 256*Fs) but the clock are to low.
We use on our board an external resonator of 24.576MHz.
Any idea of the problem?
Let me know.
Thanks.
Silvio.