Hello,
I am using TLV320AIC3106 . It is interfaced via I2S with am335x. I am using SITARA sdk.
The LINE1LP , LINE1RP, LINE 2LP, LINE2RP are connected to different audio signals(single ended). I wants to enable one input at a time (eg. If I2S input enabled then all other input signals should be disable. same as, if LINE 1L enabled then all other inputs should be disable). I wants to do this using ALSA. I tried some of the commands of amixer which are mentioned bellow but not working for me.
amixer sset 'Left PGA Mixer Line1L' on
amixer sset 'Left PGA Mixer Line2L' off"
amixer sset 'Left PGA Mixer Line1R' off"
amixer sset 'Right PGA Mixer Line1R' off"
amixer sset 'Right PGA Mixer Line1L' off"
amixer sset 'Right PGA Mixer Line2R' off"
please, can anyone help me to resolve this problem?
thanks in advance
Rajesh