Hi all:
I have two question about PCM1794A output waveform.
First, I have to use PCM1794A (Digital Filter Bypass Mode) to replace PCM1704 for my case.
Cause I have designed digital filter and that PCM1794A internal filter will crash my function, I have to use Digital Filter Bypass Mode.
I try to use MONO standard 24-b Mode, the performance must be grate!
So that I change the mode to Digital Filter Bypass Mode (MONO).
Start my controller, I find that only R-channel has differ voltage output.
Q1: Can I use L-channel in Digital Filter Bypass Mode?
Second. In the Digital Filter Bypass Mode, I saw a confusing waveform as below:
Vary serious noise can crash my performance.
There is a more interesting experiment.
I short the DATA(pin 5) ground. Saying in other word, put the DATA always 0x000000.
Finally, I got the waveform as blow figure.
I measure all OP section until I/V section. I found the problem should be generated by DA.
It has serious ripple, this incredible thing let me a headache.
Q2: Could you please tell me why and how to solve this problem?
Thank you vary much.
BR,
Ocean