Hi
I wish the data sheet had more info so that I don't need to bother you guys with these straight forward questions:
1. The DS says that the sampled data widths can be 16/20/24/32-Bit Data. But no-where can I find the actual data resolution of the ADC/DAC. Is it the same as the data widths or is it fixed 16 or 24 bit?
2. There is very little information regarding the dual rate mode. For example if I am using the dual rate mode for a sampling rate of 96kHz then is the analog input actually sampled at 96kHz with a use-full signal bandwidth of 48kHz or is the signal bandwidth still 24kHz? That is does the signal bandwidth scale with the sampling rate? What about the decimation and other filters?
Thanks and regards
Manjula