Hi!
I am considering using the TLV320DAC3100 to drive the inputs to a speaker amp via AC coupling.
I need to know what the peak-to-peak voltage at the speaker output of the 3100 device would be if it was driving into a 20k ohm load (i.e. the input resistance of the Amp plus the capacitor in series are roughly 20k).
The input to the Amp needs to be at least 3.6 Vp-p.
However, the charts on the datasheet do not indicate if the 3100 can produce this output voltage.
Can someone please clarify this?
Any recommendation here will be most appreciated!
Thanks,
James