I have followed the reference design as closely as I possibly could for the PCM3070. After getting my board back and connecting it together, I get a VERY loud hum at line out. I have it connected to an amplifier to test audio and after measuring with an oscilloscope, it exactly 60Hz which I can assume is like a ground loop, even though shorting GND and CHASSIS does not help. I am relatively new to audio, including the PCM3070 chip and would love to know what is going on.
As of right now, I cannot get the Hum to turn off nor can I get any audio to pass through.
Also; I cant use PurePath since its only for people that use the exact same setup as the eval boards, so if anyone has additional scripts (for example: Analog pass through) I would be very thankful.
Thank you!