Hi,
I need help, for linux driver for the TLV320AIC3268 device.
Anyone can help me?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I need help, for linux driver for the TLV320AIC3268 device.
Anyone can help me?
Hi, Francesco,
Welcome to e2e, and thanks for your interest in our products!
All our information on drivers are in this wiki entry.
-d2
Hi Don,
I need your help, please.
I have tryed to compile your driver tlv320aic32x4.c, tlv320aic32x4.h to create a new kernel module.
All steps, that I have execute, are here : sites.google.com/.../cross-compiling-linux-kernel-module
At the end, I have find some error, when compiling your source code, see attached images.
why this errors?
Can you help me? I need to work with this codec: - tlv320aic3204
My idea is to create the new module to add on the board at my kernel . I use the Angstrom distribution.
I await your reply,
Best regards,
Ing. Francesco.
PS
anyway, the way to work correctly with the codec driver, is correct. The Angstrom release, load automatically the audio codec:ti,audio-codec = <&tlv320aic3x>;
How to switch to my new driver?
the step are correctly?
1) create the new drive, through new module, compiling tlv320aic32x4.c, tlv320aic32x4.h without error
2) add new module to the kernel, that run on BBB board
3)change the dts file, that include tlv320aic32x4, compiling dts and crate dtbo
4)disable BB-BONELT-HDMI
5)load the DT file for Audio Cape
6)run ALSA
Are correct, is possible?