This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Confirmation on using SRC4184

Other Parts Discussed in Thread: SRC4184, SRC4192

Hi,

Our system requires interfacing Bluetooth module audio to and audio mixer using I2S interface.  The Bluetooth module support only 8KHz sampling rate with 16-bit data width over a 24/32-bit frame (I2S format).  The mixer will support sampling rates from 32KHz onwards. For this we are planning to interface these modules through SRC4184.  The BT module will not be sending the data continuously and this depends on the BT paired device.  The mixer expects a continuous stream of data on the I2S and mixer will act only as slave over the I2S bus.

Please suggest if SRC4184 can be used in this scenario.

Thanks and Regards,

Manesh