I have looked through the forum and wiki. I have read the data sheet. I am new at using an audio converter. I believe that my connections are all correct. The TLV320DAC3100 is being used as a slave. My processor is supplying the MCLK, WCLK, DIN and BCLK. What I do not understand is all of the register settings. I am having a difficult time understanding the register settings connection to the wave file settings. I would like to use the GPIO1 output to check my register settings. We are playing a wave file from an SD card. The audio is coming out of the speaker but it is speeded up.
Looking at page 48 of the datasheet how do I relate the DAC MAC and DAC_fs to the register settings? There seem to be a lot of settings that have to be correct and any one of them could cause a problem. How can I check the settings for correctness?
Can I use the GPIO1 out to check my settings?