Hi everyone . This is my first post in TI forum .
I am using TLV320AIC23BPW and i was wondering if you can answer my questions.
I am using this CODEC in USB mode (12 MHz Crystal for MCLK) and DSP Mode Digital Interface
and only Slave mode (only DAC). My Questions are :
1 - I would not use nor analog Line and neither Microphone Inputs . Should i tied these inputs to the GND ?
2 - My Digital Interface has a 5 MHz BCLK from a FPGA and this clock is not synched with input clock of CODEC . Should i use CLKOUT pin of CODEC to synchronize BCLK with CODEC input MCLK ?
3 - There is a lot of options for selecting MCLK and DAC filters. To achieving for the best sound quality from this CODEC what MCLK must be chose ? I can use 96KHz Sample Rate for 32-bit or 24-bit data length.
Thanks for your support.