Hi,
The capless pseudo differential configuration for the TLV320AIC34 is not completely clear to me.
Today we apply the following configuration:
Register 14: D7 = 0 capless mode, D6 = 0 no fully differential output
Register 37: D5-D4 = 01: HPLCOM_x configured as constant VCM output
Register 38: D5-D3 = 100: HPRCOM_x configured as external feedback with HPLCOM_x as constant VCM output
Please note that HPLCOM and HPROM are shortcut.
Register 51: unmute, select high impedance for power down and power ON driver for HPLOUT
Register 58: unmute, select high impedance for power down and power ON driver for HPLCOM
Register 65: unmute, select high impedance for power down and power ON driver for HPROUT
Register 72: unmute, select high impedance for power down and power ON driver for HPRCOM
I noticed that it doesn’t make a difference if I keep the HPLCOM and HPRCOM drivers not powered and muted.
Why doesn’t it make a difference and which setting do you recommend?
Thanks
Thomas