I originally posted this question to Ti's support and was redirected to send it through their distributors. Said distributors failed to gain me a reply after weeks orf reminders. Ti then directed me to post it here on this forum so that their experts can deal with it. What a rigmarole! Anyway, here goes, in the hope that someone can give me an answer.
Problem:
I need to design a low chip count transmit/receive system for an audio signal using optical fibres. I'm considering using an ADC/DAC pairing at each end but don't want to have to use processors if I can avoid it. I hit on the idea of using your PCM4201 with DIT4096 for the transmit side (with suitable buffering and optical transmitter) but am not clear about what to use for the receive end. I'm hoping you can advise. A bonus would be if there was a way of adding a couple of logic signal bits but that's not mandatory as I can signal them using a high audio frequencies above the telephony band. Power is not an issue, BTW. Any ideas or suggestions? Thanks for your time