Hi all, i am trying to do the following
S/PDIF (96 kHz) center tapped input on RXIN0-->DIR-->DIT-->MPO0
here are the rgisters i am setting:
23h@0x00
34h@0x00
42h@0x22
60h@0x11
78h@0x0D
I get a NON valid S/PDIF signal output any ideas why? when i check register CALCULATED SAMPLE FREQUENCY says out of range?