Hi Everyone,
I have a similar question to the one being raised before in this forum, but didn't received an answer as far as I could see.
I am trying to enable loopback feature on my TLV320AIC34 EVM board, using the script provided with the installation CD, but it doesn't work.
After reading this forum, I saw that I need to short J17A pins 11 and 13 (Din_A and Dout_A) in order to use the on-board MIC, and also set SW to USB mode instead of I2S.
I did both, and also try to set WCLK and BCLK to output as suggested, but it didn't work as well.
Can someone offer some ideas?
Thanks,
Tzviel