Hello,
I've installed PurePath Console 3, which has listed "generic I2C devices" since TLV320AIC3254 is not listed anywhere else. In this case I assume this Console 3 is the correct one for TLV320AIC3254/3204 devices.
After the installation I've the attached screenshot and when I click on I2C Master rectangle, I'll get only some simple window where I can type something and that's all.
1. Can you please guide me how can I select the device and get some user friendly environment where I can do the PLL settings and get the filter coefficient in the same way like it was in PurePath Studio version released around 2009?
2. To avoid this software at this moment, can you advice me how to calculate D register value for PLL settings in TLV320AIC3204 to get the fractional output? I've 12.5MHz MCLK input and I need to get 44.1kHz and 16kHz sample rates. I'd say at this point it's easier to get the formula to calculate it instead of installing such a complicated PurePath Console.
Thank you,
Daniel