|
|
|
|
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
|
|
|
|
Please find the details.
Input settings:
Line1L is configured as single ended. LINE1L is connected to the left ADC PGA .Input level control gain = 0dB.( Reg 19,page 0)
Gain settings: Left ADC PGA gain settings:22dB ( Reg 15,page 0)
Output Settings:
DAC_L1 is routed to HPLOUT. HPLOUT Output Level Control =9dB (( Reg 51,page 0)
Audio input level set at 35mVp.(I have captured the audio output at HPLOUT in audio analyser and verified that there is no clipping.)
The audio input is fed at LINE1LP and the looped back audio output at HPLOUT is fed to audio analyser.
I am attaching the schematic of the board and a screen shot of the register values of the codec for page 0 captured.
With reference to the Schematic,I am using Handset_MIC to input the tone and Handset_SPK to capture the output.
I would like to know what is the passband attenuation at 0.45fs for DAC Interpolation filter.
This is the frequency response observed.
Input Audio Signal : 35mVp |
|||
fs @8KHz |
fs @12KHz |
||
Input Audio |
Output Amplitude |
Input Audio |
Output Amplitude |
1 |
978 |
1 |
1014 |
1.2 |
950 |
1.2 |
1004 |
1.3 |
933 |
1.3 |
997 |
1.4 |
912 |
1.4 |
990 |
1.5 |
890 |
1.5 |
982 |
1.6 |
868 |
1.6 |
973 |
1.7 |
843 |
1.7 |
964 |
1.8 |
817 |
1.8 |
954 |
1.9 |
790 |
1.9 |
944 |
2 |
762 |
2 |
931 |
2.18 |
771 |
2.5 |
855 |
2.2 |
733 |
2.7 |
820 |
2.3 |
670 |
3.28 |
771 |
2.4 |
638 |
3.5 |
661 |
2.5 |
606 |
4 |
550 |
3 |
430 |
5 |
297 |
3.6 |
157 |
5.4 |
157 |
Expecting 3dB cut off frequency at 3.6KHz (0.45fs) Observed 3dB cut off at 2.18 KHz |
Expecting 3dB cut off frequency at 5.4KHz (0.45fs) Observed 3dB cut off at 3.28 KHz |
Hi Luis Fernando Rodríguez
I tried to test with 0.707 mVrms with zero internal gain.but I got the same observations.
I was using the Linux audio test application which was part of the BSP of AM1808 for audio loopback test.
In order to isolate the LInux audio test application application from the test scenario,
We tried to develop the drivers for the codec in Code composer studio using the the AM1808 evm (it has the same codec ).
I have done the same loopback test in JTAG mode with the custom driver we developed.
Frequency response meets the specifications.
Now I have to implement the same in our board.
Will keep you updated once we finish debugging in our board.
Thank you
Hi Luis
kindly view this post as a continuation of the thread.
I have configured the codec at 8KHz sampling rate using the custom software we developed in JTAG.
I am feeding a sine wave of frequency 1 KHz using audio signal generator and I do McASP loopback on the processor side.(Kindly refer the test setup in the previous post for clarification)
I get the specified response both in terms of amplitude and frequency for a range of input amplitudes from 20mVp to 80 mVp and frequency from 500 Hz to 3.4 KHz.
I have kept the Analog PGA gain at 55 corresponding to the register value of 0x37.
Problem Statement
In the same setup,I tried to enable AGC.
I have kept the target level as -5.5dB.
It keeps the amplitude of the output ( as observed on audio loopback ) 5.5 dB down the full scale for the range of inputs 10 mVp to 80mVp.
But I observe a fluctuation in the amplitude of the sinewave loopbacked output even though the input amplitude and frequency is kept constant.
The amplitude varies by around 1 dB in time. Ie It goes down by 1dB , then increases to the expected level and again go down by 1dB so on. Correspondingly the register values of Register 32 ie Left Channel Gain Applied by AGC Algorithm changes by 1 dB.
I have changed the attack and decay times between both extremes..But I am not able to eliminate the fluctuation completely.
In the same input conditions, If I disable the AGC,I get a constant amplitude output as set by the PGA gain.
Kindly give your suggestions to eliminate the fluctuation observed.
Luis
sorry about the delayed response.
Please have a look at the register values from the text file attached. It is the test code used in the setup.
Rest of the registers are left at the default values.
I will consolidate the values for ease of understanding.
1.PLL is disabled. sampling clock derived from 24.576 MHz crystal.Please refer schematic from earlier posts.clock configuration is correct since frequency response matches the specified response for different sampling rates.
2.sampling rate for test setup set at 8KHz.
3. left DAC datapath plays left channel input data
4.codec configured as master.
5.input given at Line1LP and output taken from HPLOUT.
6. LineL1 routed to Left AGC ,Left AGC to Left ADC. the looped back digital data from left ADC fed to left DAC.DAC_L1 is routed to HPLOUT.
7.input amplitude: 20mVp to 80 mVp
8.input frequency range:500 to 3.4 KHz
9. fs(ref) = 48kHz (for AGC time constant.)
10.target level -5.5dB.
Kindly suggest recommended values for attack and release times so that I can eliminate the fluctuation.
/*#################################################################################### # # File Name: SDRMP_AudioCodec.c # ####################################################################################### # # Project Name : SDR-MP # # Project Code : # # Created : # # Purpose : Implementation of LV320AIC3106 functions for OMAP-L138. # # Description : # # Author(s) : Shino Samuel # # Version No : # # Revisions : # # Remarks : Complete # # Copyright : Centre for Development of Advanced Computing(C-DAC), Trivandrum - 2011 #########################################################################################*/ #include "main.h" #include "SDRMP_McASP.h" #include "SDRMP_Types.h" #include "SDRMP_OMAPL138.h" #include "SDRMP_Global.h" #include "SDRMP_ISRs.h" #include "SDRMP_AudioCodec.h" uchar ReadVal[5] = {0xFF, 0xFF, 0xFF, 0xFF, 0xFF}; /*################################################################### # # Function Name: AIC3106_Init # ##################################################################### # # Arguments : # # Description : Initialise AIC3106 codec chip. # # Return Type : int # # Remarks : complete # ###################################################################*/ #define AGC_EN //#define Analog_Passthru int AIC3106_Init() { int i=0; int Test_Value; // select page 0 and reset codec. AIC3106_WriteRegister(AIC3106_REG_PAGESELECT, 0); do { AIC3106_WriteRegister(AIC3106_REG_RESET, 0x80); for(i=0; i<=100000; i++){}; AIC3106_ReadRegister(AIC3106_REG_RESET, ReadVal); } while(!(ReadVal[0] == 0)); // config codec regs. please see AIC3106 documentation for explanation. // Document Num: TLV320AIC3106 AIC3106_WriteRegister(3, (0 << 7) | // PLL is disabled (4 << 3) | // PLL Q value = 4 (2 << 0)); // PLL P value = 2 AIC3106_WriteRegister(2, (0xA << 4) | // ADC fs = fs(ref)/6 (0xA << 0)); // DAC fs = fs(ref)/6 AIC3106_WriteRegister(7, (0 << 7) | // fs(ref) = 48kHz (needed only for AGC time constants, not used) (0 << 6) | // ADC dual rate mode is disabled (0 << 5) | // DAC dual rate mode is disabled (1 << 3) | // left DAC datapath plays left channel input data (0 << 1) | // right DAC datapath plays right channel input data (0 << 0)); // reserved //0x04); AIC3106_WriteRegister(8, (1 << 7) | // BCLK is output (use "1" for output) (1 << 6) | // WCLK is output (use "1" for output) (0 << 5) | // do no place DOUT in high-z when inactive (0 << 4) | // BCLK & WCLK disabled in master mode if code powered down (0 << 3) | // reserved (0 << 2) | // disable 3D effect (0 << 0)); // digital mic support disabled AIC3106_WriteRegister(9, (0 << 6) | // serial data bus in i2s mode (0 << 4) | // audio word length 32 bits//0 - 16bit,3 - 32bits (0 << 3) | // continuous transfer mode (0<< 2) | // don't resync DAC w/ group delay variation (0 << 1) | // don't resync ADC w/ group delay variation (0 << 0)); // resync w/o soft muting //0x30); // I2S mode, 32-bit data words, continous xfer mode AIC3106_WriteRegister(12,0x00);//filter AIC3106_WriteRegister(101, (0 << 6) | // read only (0 << 5) | // MFP3 pin as GPI disabled (0 << 3) | // read only (0 << 2) | // MFP2 pin as GPO disabled (0 << 1) | // MFP2 drives low when configured as GPO (1 << 0)); // CODEC_CLKIN uses CLKDIV_OUT //0x01); AIC3106_WriteRegister(102, (0 << 6) | // CLKDIV_IN uses MCLK (0 << 4) | // PLLCLK_IN uses MCLK (0 << 0)); // PLL clock divider N = 16 //AIC3106_WriteRegister(10, 0x00); // data word offset AIC3106_WriteRegister(17,0xFF); // MIC3L/R not connected to Left ADC AIC3106_WriteRegister(26,0x80); for(i=0; i<=100000; i++); AIC3106_WriteRegister(28,0x8D); for(i=0; i<=100000; i++); AIC3106_WriteRegister(27, 0x31); for(i=0; i<=100000; i++); AIC3106_WriteRegister(34,0xF9); for(i=0; i<=100000; i++); AIC3106_WriteRegister(103,0x7C); for(i=0; i<=100000; i++); AIC3106_WriteRegister(104,0x7C); for(i=0; i<=100000; i++); AIC3106_WriteRegister(19, (0 << 7) | (0 << 3) | (1 << 2) |// left ADC is powered up(1) (3 << 0));//soft stepping disabled AIC3106_WriteRegister(20,0xF0); // MIC3L/R not connected to Left ADC AIC3106_WriteRegister(21,0x78); // MIC3L/R not connected to Left ADC AIC3106_WriteRegister(22, (0 << 7) | (0 << 3) | (0 << 2) |// right ADC is powered up (1) (0 << 0)); AIC3106_WriteRegister(37, (1 << 7) | // left DAC powered up (0 << 6) | // right DAC powered up (2 << 4) | // HPLCOM configured as independent single-ended output (not used here) (0 << 0)); // reserved //0xE0); AIC3106_WriteRegister(38, (0 << 3) | // HPRCOM configured as differential of HPROUT (0 << 2 ) | // Short circuit protection on all high power output drivers is disabled (0 << 1) | // If short circuit protection enabled, it will limit the maximum current to the load (0 << 0)); // reserved //0xE0); // set the DAC gain AIC3106_WriteRegister(43, (0 << 7) | // left DAC channel is not muted (0 << 0)); // left DAC gain setting = 0dB AIC3106_WriteRegister(44, (1 << 7) | // right DAC channel is not muted (0 << 0)); // left DAC gain setting = 0dB #if 0 // set the DAC gain AIC3106_WriteRegister(43, (0 << 7) | // left DAC channel is not muted (0x28 << 0)); // left DAC gain setting = -20dB AIC3106_WriteRegister(44, (0 << 7) | // right DAC channel is not muted (0x28 << 0)); // left DAC gain setting = -20dB #endif #ifdef Analog_Passthru /*Start of HPLOUT Output Level Configuration*/ AIC3106_WriteRegister(46, (1 << 7) | // DAC_L1 is routed to HPLOUT (0 << 0)); // DAC_L1 to HPLOUT analog volum control //0x80); #endif /*Start of HPLOUT Output Level Configuration*/ AIC3106_WriteRegister(47, (1 << 7) | // DAC_L1 is routed to HPLOUT (0 << 0)); // DAC_L1 to HPLOUT analog volum control //0x80); AIC3106_WriteRegister(51, (0 << 4) | // HPLOUT output level control = 0dB (1 << 3) | // HPLOUT is not muted (0 << 2) | // HPLOUT is weakly driven to a common-mode when powered down (0 << 1) | // read only (1 << 0)); // HPLOUT is fully powered up // 0x09); /*End of HPLOUT Output Level Configuration*/ /*Start of HPROUT Output Level Configuration*/ AIC3106_WriteRegister(61, (1 << 7) | // DAC_L1 is routed to HPROUT (0 << 0)); // DAC_L1 to HPROUT analog volum control //0x80);; AIC3106_WriteRegister(65, (0 << 4) | // HPROUT output level control = 0dB (1 << 3) | // HPROUT is not muted (0 << 2) | // HPROUT is weakly driven to a common-mode when powered down (0 << 1) | // read only (1 << 0)); // HPROUT is fully powered up // 0x09); /*End of HPROUT Output Level Configuration*/ /*Start of LEFT_LOP/M Output Level Configuration*/ AIC3106_WriteRegister(82, (1 << 7) | // DAC_L1 is routed to LEFT_LOP/M (0 << 0)); // DAC_L1 to LEFT_LOP/M analog volum control //0x80); AIC3106_WriteRegister(86, (0 << 4) | // LEFT_LOP/M output level control = 0dB (1 << 3) | // LEFT_LOP/M is not muted (0 << 2) | // reserved, read only (0 << 1) | // read only (1 << 0)); // read only (must write 1 for some reason) // 0x09); /*End of LEFT_LOP/M Output Level Configuration*/ /*Start of RIGHT_LOP/M Output Level Configuration*/ AIC3106_WriteRegister(89, (1 << 7) | // DAC_L1 is routed to RIGHT_LOP/M (0 << 0)); // DAC_L1 to RIGHT_LOP/M analog volum control //0x80); AIC3106_WriteRegister(93, (0 << 4) | // RIGHT_LOP/M output level control = 0dB (1 << 3) | // RIGHT_LOP/M is not muted (0 << 2) | // reserved, read only (0 << 1) | // read only (1 << 0)); // read only (must write 1 for some reason) // 0x09); /*End of RIGHT_LOP/M Output Level Configuration*/ return SUCCESS; } /*################################################################### # # Function Name: AIC3106_WriteRegister # ##################################################################### # # Arguments : Addr, Data # # Description : Write register AIC3106 codec chip. # # Return Type : int # # Remarks : complete # ###################################################################*/ int AIC3106_WriteRegister(uchar Reg_Addr, uchar Data) { int32 lint32_Rtn = 0, i=0; uchar i2c_data[2]; for (i=0;i<100;i++); i2c_data[0] = Reg_Addr; i2c_data[1] = Data; lint32_Rtn = int32_I2CWrite(I2C0, I2C_AUDIO_CODEC_ADDR, i2c_data, 2, SET_STOP_BIT_AFTER_WRITE); return (lint32_Rtn); } /*################################################################### # # Function Name: AIC3106_ReadRegister # ##################################################################### # # Arguments : Addr, DataBuff # # Description : Read register AIC3106 codec chip. # # Return Type : int # # Remarks : complete # ###################################################################*/ int AIC3106_ReadRegister(uchar Reg_Addr, uchar *DataBuff) { int32 lint32_Rtn = 0; // write the register address that we want to read. lint32_Rtn = int32_I2CWrite(I2C0, I2C_AUDIO_CODEC_ADDR, &Reg_Addr, 1, SKIP_STOP_BIT_AFTER_WRITE); if (lint32_Rtn != SUCCESS) return (lint32_Rtn); // clock out the register data. lint32_Rtn = int32_I2CRead(I2C0, I2C_AUDIO_CODEC_ADDR, DataBuff, 1, SKIP_BUSY_BIT_CHECK); return (lint32_Rtn); }
/*#################################################################################### # # File Name: SDRMP_AudioCodec.c # ####################################################################################### # # Project Name : SDR-MP # # Project Code : # # Created : # # Purpose : Implementation of LV320AIC3106 functions for OMAP-L138. # # Description : # # Author(s) : Shino Samuel # # Version No : # # Revisions : # # Remarks : Complete # # Copyright : Centre for Development of Advanced Computing(C-DAC), Trivandrum - 2011 #########################################################################################*/ #include "main.h" #include "SDRMP_McASP.h" #include "SDRMP_Types.h" #include "SDRMP_OMAPL138.h" #include "SDRMP_Global.h" #include "SDRMP_ISRs.h" #include "SDRMP_AudioCodec.h" uchar ReadVal[5] = {0xFF, 0xFF, 0xFF, 0xFF, 0xFF}; /*################################################################### # # Function Name: AIC3106_Init # ##################################################################### # # Arguments : # # Description : Initialise AIC3106 codec chip. # # Return Type : int # # Remarks : complete # ###################################################################*/ #define AGC_EN //#define Analog_Passthru int AIC3106_Init() { int i=0; int Test_Value; // select page 0 and reset codec. AIC3106_WriteRegister(AIC3106_REG_PAGESELECT, 0); do { AIC3106_WriteRegister(AIC3106_REG_RESET, 0x80); for(i=0; i<=100000; i++){}; AIC3106_ReadRegister(AIC3106_REG_RESET, ReadVal); } while(!(ReadVal[0] == 0)); // config codec regs. please see AIC3106 documentation for explanation. // Document Num: TLV320AIC3106 AIC3106_WriteRegister(3, (0 << 7) | // PLL is disabled (4 << 3) | // PLL Q value = 4 (2 << 0)); // PLL P value = 2 AIC3106_WriteRegister(2, (0xA << 4) | // ADC fs = fs(ref)/6 (0xA << 0)); // DAC fs = fs(ref)/6 AIC3106_WriteRegister(7, (0 << 7) | // fs(ref) = 48kHz (needed only for AGC time constants, not used) (0 << 6) | // ADC dual rate mode is disabled (0 << 5) | // DAC dual rate mode is disabled (1 << 3) | // left DAC datapath plays left channel input data (0 << 1) | // right DAC datapath plays right channel input data (0 << 0)); // reserved //0x04); AIC3106_WriteRegister(8, (1 << 7) | // BCLK is output (use "1" for output) (1 << 6) | // WCLK is output (use "1" for output) (0 << 5) | // do no place DOUT in high-z when inactive (0 << 4) | // BCLK & WCLK disabled in master mode if code powered down (0 << 3) | // reserved (0 << 2) | // disable 3D effect (0 << 0)); // digital mic support disabled AIC3106_WriteRegister(9, (0 << 6) | // serial data bus in i2s mode (0 << 4) | // audio word length 32 bits//0 - 16bit,3 - 32bits (0 << 3) | // continuous transfer mode (0<< 2) | // don't resync DAC w/ group delay variation (0 << 1) | // don't resync ADC w/ group delay variation (0 << 0)); // resync w/o soft muting //0x30); // I2S mode, 32-bit data words, continous xfer mode AIC3106_WriteRegister(12,0x00);//filter AIC3106_WriteRegister(101, (0 << 6) | // read only (0 << 5) | // MFP3 pin as GPI disabled (0 << 3) | // read only (0 << 2) | // MFP2 pin as GPO disabled (0 << 1) | // MFP2 drives low when configured as GPO (1 << 0)); // CODEC_CLKIN uses CLKDIV_OUT //0x01); AIC3106_WriteRegister(102, (0 << 6) | // CLKDIV_IN uses MCLK (0 << 4) | // PLLCLK_IN uses MCLK (0 << 0)); // PLL clock divider N = 16 //AIC3106_WriteRegister(10, 0x00); // data word offset AIC3106_WriteRegister(17,0xFF); // MIC3L/R not connected to Left ADC AIC3106_WriteRegister(26,0x80); for(i=0; i<=100000; i++); AIC3106_WriteRegister(28,0x8D); for(i=0; i<=100000; i++); AIC3106_WriteRegister(27, 0x31); for(i=0; i<=100000; i++); AIC3106_WriteRegister(34,0xF9); for(i=0; i<=100000; i++); AIC3106_WriteRegister(103,0x7C); for(i=0; i<=100000; i++); AIC3106_WriteRegister(104,0x7C); for(i=0; i<=100000; i++); AIC3106_WriteRegister(19, (0 << 7) | (0 << 3) | (1 << 2) |// left ADC is powered up(1) (3 << 0));//soft stepping disabled AIC3106_WriteRegister(20,0xF0); // MIC3L/R not connected to Left ADC AIC3106_WriteRegister(21,0x78); // MIC3L/R not connected to Left ADC AIC3106_WriteRegister(22, (0 << 7) | (0 << 3) | (0 << 2) |// right ADC is powered up (1) (0 << 0)); AIC3106_WriteRegister(37, (1 << 7) | // left DAC powered up (0 << 6) | // right DAC powered up (2 << 4) | // HPLCOM configured as independent single-ended output (not used here) (0 << 0)); // reserved //0xE0); AIC3106_WriteRegister(38, (0 << 3) | // HPRCOM configured as differential of HPROUT (0 << 2 ) | // Short circuit protection on all high power output drivers is disabled (0 << 1) | // If short circuit protection enabled, it will limit the maximum current to the load (0 << 0)); // reserved //0xE0); // set the DAC gain AIC3106_WriteRegister(43, (0 << 7) | // left DAC channel is not muted (0 << 0)); // left DAC gain setting = 0dB AIC3106_WriteRegister(44, (1 << 7) | // right DAC channel is not muted (0 << 0)); // left DAC gain setting = 0dB #if 0 // set the DAC gain AIC3106_WriteRegister(43, (0 << 7) | // left DAC channel is not muted (0x28 << 0)); // left DAC gain setting = -20dB AIC3106_WriteRegister(44, (0 << 7) | // right DAC channel is not muted (0x28 << 0)); // left DAC gain setting = -20dB #endif #ifdef Analog_Passthru /*Start of HPLOUT Output Level Configuration*/ AIC3106_WriteRegister(46, (1 << 7) | // DAC_L1 is routed to HPLOUT (0 << 0)); // DAC_L1 to HPLOUT analog volum control //0x80); #endif /*Start of HPLOUT Output Level Configuration*/ AIC3106_WriteRegister(47, (1 << 7) | // DAC_L1 is routed to HPLOUT (0 << 0)); // DAC_L1 to HPLOUT analog volum control //0x80); AIC3106_WriteRegister(51, (0 << 4) | // HPLOUT output level control = 0dB (1 << 3) | // HPLOUT is not muted (0 << 2) | // HPLOUT is weakly driven to a common-mode when powered down (0 << 1) | // read only (1 << 0)); // HPLOUT is fully powered up // 0x09); /*End of HPLOUT Output Level Configuration*/ /*Start of HPROUT Output Level Configuration*/ AIC3106_WriteRegister(61, (1 << 7) | // DAC_L1 is routed to HPROUT (0 << 0)); // DAC_L1 to HPROUT analog volum control //0x80);; AIC3106_WriteRegister(65, (0 << 4) | // HPROUT output level control = 0dB (1 << 3) | // HPROUT is not muted (0 << 2) | // HPROUT is weakly driven to a common-mode when powered down (0 << 1) | // read only (1 << 0)); // HPROUT is fully powered up // 0x09); /*End of HPROUT Output Level Configuration*/ /*Start of LEFT_LOP/M Output Level Configuration*/ AIC3106_WriteRegister(82, (1 << 7) | // DAC_L1 is routed to LEFT_LOP/M (0 << 0)); // DAC_L1 to LEFT_LOP/M analog volum control //0x80); AIC3106_WriteRegister(86, (0 << 4) | // LEFT_LOP/M output level control = 0dB (1 << 3) | // LEFT_LOP/M is not muted (0 << 2) | // reserved, read only (0 << 1) | // read only (1 << 0)); // read only (must write 1 for some reason) // 0x09); /*End of LEFT_LOP/M Output Level Configuration*/ /*Start of RIGHT_LOP/M Output Level Configuration*/ AIC3106_WriteRegister(89, (1 << 7) | // DAC_L1 is routed to RIGHT_LOP/M (0 << 0)); // DAC_L1 to RIGHT_LOP/M analog volum control //0x80); AIC3106_WriteRegister(93, (0 << 4) | // RIGHT_LOP/M output level control = 0dB (1 << 3) | // RIGHT_LOP/M is not muted (0 << 2) | // reserved, read only (0 << 1) | // read only (1 << 0)); // read only (must write 1 for some reason) // 0x09); /*End of RIGHT_LOP/M Output Level Configuration*/ return SUCCESS; } /*################################################################### # # Function Name: AIC3106_WriteRegister # ##################################################################### # # Arguments : Addr, Data # # Description : Write register AIC3106 codec chip. # # Return Type : int # # Remarks : complete # ###################################################################*/ int AIC3106_WriteRegister(uchar Reg_Addr, uchar Data) { int32 lint32_Rtn = 0, i=0; uchar i2c_data[2]; for (i=0;i<100;i++); i2c_data[0] = Reg_Addr; i2c_data[1] = Data; lint32_Rtn = int32_I2CWrite(I2C0, I2C_AUDIO_CODEC_ADDR, i2c_data, 2, SET_STOP_BIT_AFTER_WRITE); return (lint32_Rtn); } /*################################################################### # # Function Name: AIC3106_ReadRegister # ##################################################################### # # Arguments : Addr, DataBuff # # Description : Read register AIC3106 codec chip. # # Return Type : int # # Remarks : complete # ###################################################################*/ int AIC3106_ReadRegister(uchar Reg_Addr, uchar *DataBuff) { int32 lint32_Rtn = 0; // write the register address that we want to read. lint32_Rtn = int32_I2CWrite(I2C0, I2C_AUDIO_CODEC_ADDR, &Reg_Addr, 1, SKIP_STOP_BIT_AFTER_WRITE); if (lint32_Rtn != SUCCESS) return (lint32_Rtn); // clock out the register data. lint32_Rtn = int32_I2CRead(I2C0, I2C_AUDIO_CODEC_ADDR, DataBuff, 1, SKIP_BUSY_BIT_CHECK); return (lint32_Rtn); }
Heloo Luis,
Thanks for the reply. As part of testing, we are providing sufficiently high input level (1Vpp), set AGC target level to -5.5dB with refernce to the full scale value and the gain much higher than required (6dB). In this case also we are seeing the out put to vary between 521.4mVrms to 493.2Vrms. We are observing this in codec loopback test mentioned earlier. Can you Please comment us on this
Thanks
Rejeesh S Raj