Is there a way to both mute the class D amplifier and set it to high impedance just like the speaker line? When the class D line is idle (no audio stimulus) and muted (page 1, register 42, bit d2 = 0) I am measuring 13.610mA in series with the SPKVDD (W5 on TLV320AIC3100EVM-U).
One more thing to point out is using the slac366a - codec control software. I don't see a menu option to mute the class D amp. Instead I have to go to the register inspector to manipulate the mute control. Is there an updated file/software to use besides slac366a?