Is there a recommended method or tool for converting the coefficient data generated from the GDE tool into a C style array?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there a recommended method or tool for converting the coefficient data generated from the GDE tool into a C style array?
Hi Kris,
If you are talking about PurePath Studio, then when you generate the code it is possible to generate a c header file with a struct that has all of the register and coefficient writes contained in it. To ensure this happens go to Tools menu at the top of the window, then select Options. A new window will appear, make sure Generate Driver Code, and Generate Driver Interface are selected. Choosing between application patches and complete applications will be the difference of getting only the coefficients for secondary sampling rates in addition header files, or getting all register writes in each header file.
Now when you save and generate the process flow, header files with a struct of the register writes will be saved to the chosen file.
Justin