Answer:
Bit D0 ADCHP ADC High Pass Filter 1=Disabled 0=Enabled Bit D2-D1 DEEMP[1:0] De-emphasis Control 00=Disabled 01=32kHz 10=44.1kHz 11=48kHz Bit D3 DACM DAC Soft Mute 0=Disabled 1=Enabled Note: 1) The ADCHP default is correct. The Data Manual was incorrect with the Disabled and Enabled values reversed. This bit does not apply to the DAC23. 2) The De-emphasis defaults are not correct in the Data Manual. The defaults should be disabled which is 00. 3) The DAC Mute is muted by Default. The Data Manual was incorrect with the DAC un-muted and it should have been defaulted to Mute. |