Dear technical support team,
I have a question about DIR of PCM9211.
Checking 0x39 for LOCK/UNLOCK and input Fs of DIR.
When S/PDIF input(LPCM44.1kHz), 0x39 shows variation like 0x08 and 0x88.
This shows both 44.1kHz sampling and during frequency calculation .
It cause once in about 10 power-on.
Following is other status.
・ERROR pin and NPCM pin always show "low".
・If remove the cable for causing unlock status and connect cable again, 0x39 shows 0x08 and stable.
・If hard reset(RST pin) or soft reset assert while 0x39 shows 0x88 and set register again, 0x39 shows 0x08 and stable.
・Using 24.576MHz XTI
・Register setting is following
Reg 0x20:0x00
Reg 0x23:0x00
Reg 0x24:0x80
Reg 0x25:0x29
Reg 0x26:0x00
Reg 0x28:0x07
Reg 0x2A:0x7F
Reg 0x30:0x10
Reg 0x31:0x0A
Reg 0x34:0xC2
Reg 0x40:0xE2
Reg 0x6B:0x11
Best Regards,
y.i