Hi,
We are working on customized board using ti-ezsdk_dm816x-evm_5_05_02_00.
I understand that TLV320AIC3x chip which is used in evm board supports 8-bit registers so the snd_soc_codec_set_cache_io(codec, 8, 8, aic3x->control_type); is using parameters 8,8.
But we are using sgtl5000 chip in our customized board and it supports 16 bit address and data registers, so 16, 16 has been used in snd_soc_codec_set_cache_io().
Whether using 16-bit , 16-bit in snd_soc_codec_set_cache_io() function parameter will cause any issue in register read/write??
Thanks in advance.
Regards,
Ambika