Hello,
I'm planning to use TLV320AIC3204 dsp. and in the datasheet, the recommended current supply be more than 150mA.
I'm currently using a 7.8V~12V power supply so linear regulator like lm1117 has a thermal problem.
So I thought TPS51225 was one option to use 3.3V for AVDD and use 5V with an LDO 1.8V for IOVDD. but the TPS51225 LDO has a max 100mA current output. Is there any reference buck controller to be used with TLV320AIC3204 When using high supply voltage?
Thanks