Hi Team,
Table 10 shows "(2) This system clock rate is supported by PLL mode" as the following, however I couldn't catch what does it indicate.
Does it correlate somewhat with Table 11?
Best Regards,
Yaita / Japan disty
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Normally on I2S is used Audio frame 64 bits long for both channels. You can have 16, 24 or 32 bit samples in them. There also exists I2S signals for 16bit samples which use only 32bit frames long or 24bit samples which used 48bit long frames.
Example for Table 11:
CD signal 16bits/44.1kHz:
BCK 64bits: 2.8224MHz
BCK: 48bits: 2.1168MHz
BCK: 32bits: 1.4112MHz
It tells, that when you use 3 wire I2S without SCK signal, that DAC accept BCK 64x, 48x or 32x FS and internally generate SCK 5.6448MHz for BCK 64x and 32x and 8.4672MHz for BCK 48x.
It mean that with BCK64x is used 2x oversampling, with BCK48x 4x and with BCK32x also 4x for 44.1kHz sample frequency.
LRCK is always sample frequency.
I always used BCK 64x FS for all sample frequencies and bit depths.
Hi
I believe (2) of Table 10 indicates internal PLL is used although 4-Wire I2S as the following.
(datasheet page 24)
The device has an internal PLL that is used to take either SCK or BCK and create the higher rate clocks required by the interpolating processor and the DAC clock.
On the other hand, the fsck value that doesn't show (2) indicate internal PLL isn't used. SCK itself is used for the higher rate clocks required by the interpolating processor and the DAC clock.
Is my understanding correct?
Best Regards,
Yaita
Hi Justin-san,
Thank you always for your support.
I would like to confirm just in case.
Is the following yellow part typo for "table 11"?
>For table 10, every scenario is using the PLL to create faster system clock.
Best Regards,
Yaita
Hi Yaita-san,
Correct, I apologize, table 11 is what I meant there.
Justin
Justin, Pavel,
Can you help me to understand this restriction?
My customer has seen that PCM510xA-Q1 does NOT operate with 128fs(12.288MHz) SCK for 96KHz sampling frequency.
From the description of 3-wire PCM mode, I suppose that the internal PLL is disabled, since customer has SCK input.
So, it means, to support 128fs for 96KHz, it's required to use 3-wire PCM mode (in other words "PLL mode".).
Correct?
Thank you so much for your support.
Regards,
Ken
Hi Paul,
What make me confused is not much description of "PLL mode" in the datasheet.
If you say that "PLL mode" means "Clock Slave Mode with BCK PLL to Generate Internal Clocks (3-Wire PCM)", then I fully understand.
Thanks,
Ken