Hi,
A customer asked us about the IOL and VOL of TLV320AIC3104 SDA pin. Can he use the value of 0.1 IOVDD as DIGITAL I/O VOL MAX when the IOL is 4 mA?
He will design i2c sink current as 4 mA. He checked TLV320AIC3104 datasheet to confirm the VOL at sink current 4mA. However, he could not find any values of IOL.
Please teach us the VOL value of SDA pin when IOL is 4 mA. Even if no one knows it, I think according to the I2C bus specification, at least the VOL of TVL320AIC3104 SDA pin is less than 0.4 V when sink current is 3 mA. Is this right?
Best regards,
Akio Ito