Hello,
I wish to use the secondary I2S interface in TLV320AIC3254, but it seems that audio chip has not enough pins to have all its signals.
As you can see on the following drawing, I use the 1st interface to communicate with a main host (input : Stereo audio data, output : microphone audio data). And I want to use the secondary I2S interface to transmit data to a DAC/Amp/Speaker chain. In this case, TLV320AIC3254 is host, so, it has to generate clocks and emits data on Dout.
My problem :
When I analyze pins available for secondary interface, I understand that I have only 2 pins (MISO, GPIO) for 3 signals (BCLK2, WCLK2, Dout2). Dout pin is already use for 1st interface.
See table 1, p.27 of TLV320AIC3254 datasheet : http://www.ti.com/lit/ds/symlink/tlv320aic3254.pdf
Can you say me if I make mistakes in my analysis ?
Have you got a solution to use the secondary I2S with Dout signal ?
Kind regards,
Fabien