Hi
I have a question about PCM5242
Question:
What is the reset value of miniDSP instruction buffer register(page 0xA0, page 160) value in PCM5242?
Issue:
Using PCM5242 to switch from 48K sampling rate to 192K sampling rate,
I find that most registers in the page 0xA0 are modified in 48K configuration file,
But only 4 registers in the page 0xA0 are modified in 192K configuration file,
when switching from 48K to 192K, page 0xA0’s modified register will affect the 192K output , so I want to know the reset value of page 0xA0’s register.Once modified to 192K ,writing reset values to page 0xA0
The configuration flow is as below(using 8X at 48K sampling rate, 2X at 192K sampling rate)